Error_Register

Error_Register

Address: 4609 (1201H)
Type: WORD
Access: Read Only
Unit: --
Range: --
Default Value: --
Store Supported: No
Description:

This object contains the state of the various drive errors.

Bit #

Name

Description

Default value

0

Protection_Drive_Thermal

1 = Drive is in thermal protection condition

0 = Ok

0

1

Protection_Drive_Voltage

1 = Drive is in voltage protection condition

0 = Ok

0

2

Protection_Drive_Current

1 = Drive is in current protection condition

0 = Ok

0

3

Protection_Open_Phase

1 = Drive is in open phase protection condition

0 = Ok

0

4

Missing_Torque_Enable

1 = Torque Enable Input Missing (only for drive with Torque Enable Input)

0 = Ok

0

5

Feedback_Error (1)

1 = Motor Feedback Error

0 = Ok

0

6

Protection_Current_Regulation

1 = Drive is in current regulation out of range protection condition.

      Verify Motor Currents

0 = Ok

0

7

Protection_Open_Transistor

1 = Drive is in open transistor condition

0 = Ok

0

8

KM Space_User_Program

1 = Kollmorgen Space User Program Error

0 = Ok

0

9

Internal_SW_Error

1 = Drive is in internal software  error condition

0 = Ok

0

10

KM Space_Software_Protection

1 = Kollmorgen Space software protection

0 = Ok

0

11

Missing_Calibration

1 = Missing Calibration

0 = Ok

0

12

Watchdog_Occurred

1 = Internal Watchdog Occurred

0 = Ok

0

13

Eeprom_Fail

1 = Eeprom Failure

0 = Ok

0

14

I2T_Protection

1 = I2T Protection

0 = Ok

0

15

Feature_Unavailable

1 = Feature unavailable

0 = Ok

0

Notes: (1) See Feedback_Status object for more details about type of Feedback Error.